Modify PLCopen Axis

A PLCopenA vendor -and product- independent worldwide association active in Industrial Control and aiming at standardizing PLC file formats based on XML axis can be modified by using the PLCopen Axis Data dialog. To display this dialog you can:

PLCopen Axis Context Menu

Figure 5-20: PLCopen Axis Context Menu

The PLCopen Axis Data dialog is displayed as follows:

PLCopen Axis Data Dialog

Figure 5-21: PLCopen Axis Data Dialog

About Axis Name and Number

The Copy function block is needed to link the Axis Number defined in the PLCopen Axis Data dialog (1 in the figure above) to the Axis Name (Axis1 in our example)

Then, this Axis Name (Axis1 in our example) is an instance of an AXIS_REF data structure that can be used in your PLC"Programmable Logic Controller" A Programmable Logic Controller, PLC, or Programmable Controller is a digital computer used for automation of industrial processes, such as control of machinery on factory assembly lines. Used to synchronize the flow of inputs from (physical) sensors and events with the flow of outputs to actuators and events programs.

see "AXIS_REF Structure"

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™